Use this client library to access the services of the Metasys Server application programming interface (API). If you want to create a new application in a .NET platform, the client library provides an easy way to access the Metasys APIs. The document describes how to install the Metasys client library and use .NET or COM to interact with the API. You will find examples of both .NET and COM provided on the Metasys Basic Services GitHub repository, for more information, see https://github.com/metasys-server/basic-services-dotnet/blob/master/README.md. You can call methods using the command line, scripts, or create an API to API integration using an open weather forecast service.
The intended audience for this document is C# and Visual Basic Application (VBA) developers, but it is not limited to those users.