The system shuts down if one of the following is true:
- The system is shutdown from the System Manager or VZC.
- All zone controllers are offline.
- The SAT sensor is unreliable.
- No voting zones are on the system.
- The system is shut down through BI-1 at the IOM selected from the SBH when the Emergency Shutdown BI is enabled.