The following scenarios represent nonvoting conditions:
- The zone temperature is unreliable.
- The zone temperature remains more than 3 degrees from setpoint for more than the user-set time period, the default is 60 minutes. For zone controllers with local heat, the time period begins when the local heat is at the maximum level. In unoccupied mode, the time period is reset.
Note: This situation only applies to occupied operation.
- The zone controller is currently offline.
- The zone vote is not allowed via the user setup; this restriction is set by the Zone Vote Allowed parameter in the Control Setup screen under the zone.
- The zone weight of a zone is set to zero.
On zones containing local heat, local heat must be at the maximum level before the zone votes for heat.