The VZC uses zone votes to direct the Verasys system to use the appropriate operating mode. This system operating mode determines the COBP RTU state, the effective occupancy, and unit-enabled attributes.
The RTU can be in one of the following states:
- Idle
- SD Alarm
- Purge Command
- Self Test
- Morning Warm-Up
- Air Tempering
- Dehumidification
- Heating
- Cooling
- Economizer
- Fan Only
- Comfort Ventilation
- Startup Delay
Locate the Unit Status Parameter on the VZC homepage or on the Circle of Comfort on the RTU Homepage. This parameter displays the current state of the RTU.