You can configure each zone to add weight so that its vote is more important than other zones. Adjust the Zone Weight parameter from the Control Setup section of the Zone View. Votes can be adjusted from 0 to 3. Zero implies it does not vote. Three implies the vote is worth three votes. The default is set to one vote.