Shut down the system in the following two ways:
- Instant Shutdown: The application performs an Instant Shutdown on heating, cooling, and the fan when the input is set to Shutdown. Minimum On timers are ignored in this mode.
-
Control Mode: The application
performs a shutdown on heating, cooling, and the fan when the Control Mode input is
Off. Minimum On timers are observed in this mode. Table 1 provides minimum on and off times for
each stage of staged heating and cooling. Note: The SMART Equipment board can have additional Minimum On timers for the compressors that must expire before the equipment shuts down. These Minimum On times exist on the VEC controller. This instance applies even if instant shutdown or control mode was used to shut off the unit.
Table 1. Minimum On and Off Times for RTU Stages RTU Stage Minimum On Time Minimum Off Time Heating 2 min 2 min Cooling 3 min 5 min
RTU
All heating and cooling is off. The supply fan is off.
Zone Damper
The zone dampers are set to 100% open.
Bypass damper
The bypass damper is set to 50% open. This value is not overridden by the value set for the maximum bypass damper position parameter.