The maximum position setting (Damper Max Position) helps to limit the amount of air bypassed on systems with oversized bypass dampers. The maximum bypass damper position only affects the limits when the bypass damper is performing duct static pressure control. When the system is off, the bypass damper is set to 50% open regardless of the maximum bypass damper position setting.