USB Port - Verasys - LC-SBH100-0 - LC-SBH100-1 - LC-SBH100-1SE - Supervisory controller - SBH100

Verasys Smart Building Hub (SBH) Installation Guide LC-SBH100-x

Brand
Verasys
Product name
SBH100
Document type
Installation Guide
Part number
24-10737-00202
Document revision
B
Revision date
2021-03-26
Product status
Active
Language
English
Note: USB port functionality is not available in this software release.

The USB port on the Smart Building Hub is a 5-pin, Micro-B peripheral serial port which conforms to the USB 2.0 standard. The Smart Building Hub USB port is for connecting to a computer for commissioning, downloading, and retrieving data. When the Smart Building Hub is connected and powered from the USB port, FC bus functions are not available.

Note: The USB connection on the Smart Building Hub is not designed for constant use. The USB port should be used only when needed.
Table 1. USB Port Pin Designations
Pin Number (Both Ends of Cable) Signal Name
1 +5 VDC
2 Data -
3 Data +
4 No Connection
5 Ground