About this task
Important: If you are going to use the Smart Building Hub on Ethernet, you must plug it
into external power before you attach the field bus adapter. See External Power Supply Connections.
Procedure
-
Connect the FC Bus port of the Smart Building Hub to the field bus port of the equipment controller using the supplied RJ-12 cable or field bus adapter. The Smart Building Hub's LEDs flash, indicating that the device is initializing. When the Fault LED turns off and the Wi-Fi LEDs flash in succession, the Smart Building Hub is ready to use .
Figure 1. Connecting the Smart Building Hub to Your Equipment
Table 1. Lighting Connections Conductor From To Wire No. Size AWG Color 1 24 White/Green P1-1 P2-4 2 24 Green P1-2 P2-3 3 24 Orange/White P1-3 P2-2 4 24 Orange P1-4 5 24 Blue/White P1-5 P2-2 6 24 Blue P1-6 - In the Wi-Fi settings of your device or laptop, connect to the Smart Building Hub Wi-Fi network using your default credentials. These credentials are included on a sticker in the Smart Building Hub Quick Start Guide (Part No. 24-10737-16) that came with your device.
-
Direct your browser to http://www.smartbuildinghub.com to open the Smart Building Hub browser
interface.
Note: Smart Building Hub ships with a private http://www.smartbuildinghub.com SSL certificate installed to ensure secure communication with the Smart Building Hub. However, this certificate does not indicate that it is trusted in a browser. If you wish to install your own certificate, refer to Adding a Private Key and Certificate to Smart Building Hub in the Smart Building Hub Network and IT Guidance Technical Bulletin (LIT-12012324).
- Read and accept the Smart Building Hub license agreement.
-
The first time you log in to the Smart Building Hub, the Change Password and Passphrase web page appears. You must change the Admin password and Wi-Fi passphrase.
Important: After you change the Wi-Fi passphrase or SSID, the web server restarts and you must rejoin the Smart Building Hub Wi-Fi network using the new passphrase. On some mobile devices, you must select and forget the original Smart Building Hub Wi-Fi network before rejoining the network with the new passphrase.
- Replace the default password in the New Admin Password field. Confirm the change by entering the new password in the Verify New Admin Password field.
- Replace the Wi-Fi Passphrase in the New Wi-Fi Passphrase field and click Save.
Results
Once the Smart Building Hub is physically connected to the MS/TP network, all the devices on the network that have unique addresses appear in the device list and are available to configure.
To interact with a device or product on the network (to view devices, set points, or view alarms), select a device using the mobile device that is connected to the Smart Building Hub.