North American emissions compliance - Verasys - LC-SBH100-0 - LC-SBH100-1 - LC-SBH100-1SE - Supervisory controller - SBH100

Verasys Smart Building Hub (SBH) Installation Guide LC-SBH100-x

Brand
Verasys
Product name
SBH100
Document type
Installation Guide
Part number
24-10737-00202
Document revision
B
Revision date
2021-03-26
Product status
Active
Language
English

United States

This equipment has been tested and found to comply with the limits for a Class A digital device pursuant to Part 15 of the FCC Rules. These limits are designed to provide reasonable protection against harmful interference when this equipment is operated in a commercial environment. This equipment generates, uses, and can radiate radio frequency energy and, if not installed and used in accordance with the instruction manual, may cause harmful interference to radio communications. Operation of this equipment in a residential area may cause harmful interference, in which case the users will be required to correct the interference at their own expense.

RF Transmitters: Compliance Statement (Part 15.19)

This device complies with Part 15 of the FCC Rules. Operation is subject to the following two conditions:

  1. This device may not cause harmful interference, and
  2. This device must accept any interference received, including interference that may cause undesired operation.

Warning (Part 15.21)

Changes or modifications not expressly approved by the party responsible for compliance could void the user’s authority to operate the equipment.

RF Exposure (OET Bulletin 65)

To comply with FCC RF exposure requirements for mobile transmitting devices, this transmitter should only be used or installed at locations where there is at least 20 cm separation distance between the antenna and all persons.

Canada

This Class (A) digital apparatus meets all the requirements of the Canadian Interference-Causing Equipment Regulations.

Cet appareil numérique de la Classe (A) respecte toutes les exigences du Règlement sur le matériel brouilleur du Canada.

RF Transmitters: Industry Canada Statement(s)

The term IC before the certification/registration number only signifies that the Industry Canada technical specifications were met.

This device has been designed to operate with an antenna having a maximum gain of [x] dB. Antenna having a higher gain is strictly prohibited per regulations of Industry Canada. The required antenna impedance is [y] ohms.

To reduce potential radio interference to other users, the antenna type and its gain should be so chosen that the Equivalent Isotropically Radiated Power (EIRP) is not more than that required for successful communication.

Le terme « IC » précédant le numéro d'accréditation/inscription signifie simplement que le produit est conforme aux spécifications techniques d'Industry Canada.

Cet appareil a été conçu pour fonctionner avec une antenne d'un gain maximum de [x] dBi. En application des réglementations d'Industry Canada, l'utilisation d'une antenne de gain supérieur est strictement interdite. L'impédance d'antenne requise est de [y] ohms.

Pour réduire les interférences radio potentielles avec les dispositifs d'autres utilisateurs, le type d'antenne et son gain doivent être choisis de façon à ce que la Puissance Isotrope Rayonnée Équivalente (PIRE) ne soit pas supérieure à la puissance nécessaire pour une bonne communication.