During startup, the Smart Building Hub automatically initiates a self-test to verify proper operation of the unit. Immediately after connecting supply power, the following LED lighting sequence occurs:
- The power LED turns on, and stays lit.
- The Fault LED indicator flashes for approximately 40 seconds, then turns off when the Smart Building Hub is fully functional.
- The Wi-Fi LEDs light up in succession (scanning), indicating that the Smart Building Hub is waiting for a device to join its Wi-Fi network.