- power
- fault
- FC bus communication
- Ethernet communication
- Wi-Fi strength
See Table 1 for a comprehensive list of Smart Building Hub LED functional information.
LED Name |
Color | Normal | Descriptions/Other Conditions |
---|---|---|---|
Power | Green | On Steady(no flashing) |
Off = No power On Steady = Power supplied by primary voltage |
Fault | Red | Off |
Off = No faults/normal operation On Steady = Missing hardware, missing software, operating system has not yet initialized, or reset is in progress. Slow Flicker (1 blink per second) = Software upgrade in progress Medium Flicker (2 blinks per second) = Startup sequence Fast Flicker (5 blinks per second) = Fault |
FC Bus | Green | Flicker |
Off = Receiving data On Steady = Transmitting data Flicker = Data transmission |
Ethernet | Green | On Steady |
Off = Communication not established On Steady = Communication established Flicker = Data transmission |
Wi-Fi | Yellow | On Steady |
Off = No Wi-Fi signal Wi-Fi strength is indicated by the number of LEDs that are lit, with one lit LED indicating weak wireless signal strength (between 1%and 49%) and three lit LEDs indicating excellent wireless signal strength (at least 75%). |