The bracket can be mounted using:
- a previously-installed DIN rail (Figure 1)
Figure 1. Positioning the Bracket on a DIN rail
- screw holes on the back of the bracket (so that the unit is flat on its back) (Figure 2)
Figure 2. Mounting Using Back-side Screws
- screw holes on the side of the bracket (Figure 3 and Figure 6)
Figure 3. Mounting Using Side Screws
- the holes in the DIN rail clips (Figure 4)
Figure 4. Mounting Using DIN Rail Screw Holes
This orientation helps accommodate on-site constraints. Screw hole locations are illustrated in Figure 5 and Figure 6.
The screw types needed to mount the unit depend upon the surface to which the unit is mounted. The screw holes on the Smart Building Hub can accommodate M3.5 and #6 screws.
For information on location considerations for maximizing signal strength, see the Location Considerations section.
To mount the bracket on a flat surface (such as a wall):
- Pull the bottom mounting clip outward to the extended position.
- Mark mounting hole locations on the wall using the dimensions shown in Figure 5 or Figure 6; or hold the bracket against the
wall and mark the hole locations through the mounting clips.Note:
- The position of the location holes depends on whether the bracket is mounted horizontally or vertically.
- The screw holes on the Smart Building Hub can accommodate M3.5 and #6 screws.
- Drill holes in the wall based on the locations marked in the preceding step, and insert wall anchors for each hole (if necessary).
- Hold the bracket in place, insert the screws through the mounting clips and into the screw holes, and then carefully tighten all screws.
Important: Do not overtightened the mounting screws. Over-tightening the screws may damage the mounting clips or bracket.
- Place the Smart Building Hub unit in the bracket and secure the bracket with the locking screw.
Figure 5. Mounting Holes, Flat-Mounting (Left) and Side-Mounting (Right)
Figure 6. Mounting Holes, Flat Mounting, DIN Rail Screws