Accessing Smart Equipment Using the Smart Building Hub - Verasys - LC-SBH100-0 - LC-SBH100-1 - LC-SBH100-1SE - Supervisory controller - SBH100

Verasys Smart Building Hub (SBH) Installation Guide LC-SBH100-x

Brand
Verasys
Product name
SBH100
Document type
Installation Guide
Part number
24-10737-00202
Document revision
B
Revision date
2021-03-26
Product status
Active
Language
English

About this task

When the Smart Building Hub is physically connected to an MS/TP network, you can have access to Smart Equipment devices. The Smart Building Hub connects through the field controller (FC) bus. From this connection it has access to the devices on the trunk.

To interact with a device or product on the network (to view devices, setpoints, or view alarms), users select the device using a web-enabled device that is connected to the Smart Building Hub Wi-Fi network. To use the network, you must have a web-enabled device that uses a supported Internet browser. For information on connecting to the network, see Connecting to the Smart Building Hub Wi-Fi Network.