To view a list of all the online and offline Verasys devices connected to the
SBH, click Devices.
Note: On the Devices page, the system bus devices and zone bus
devices appear in separate lists. See the following figure and table.
Figure 1. Devices page
Callout | Description |
---|---|
1 | A single device. To access detailed information about the device, click anywhere in the box. |
2 | If a zoning system is present, the Zone
Coordinator header appears. To view the zone bus devices
under the zone coordinator, expand the zone coordinator. Note: A single zone RTU appears in a solid blue box
without the arrow icon on the right.
|