For information about the spaces on the Lighting tab, see the following figure and table.
Figure 1. Facility lighting tab
Callout | Description |
---|---|
1 | The name of the lighting space. |
2 | Master override setting to turn the lights on or off automatically or manually. |
3 | A link to the home page of the lighting device and buttons to access the device trends and schedules. |
4 | The light control setting, for example, a schedule that you can configure. |
5 | The status of the lights. |