For information about the spaces on the HVAC tab, see the following figure and table.
Figure 1. Facility HVAC tab
Callout | Description |
---|---|
1 | One of the following HVAC statuses:
Note: The current temperature, humidity, and status of the space
change colors depending on the status.
|
2 | Occupancy status |
3 | The setting for the system mode, and the setting to turn the device on or off. |
4 | A link to the home page of the device that controls the space, and buttons to access the device alarms, schedules, and trends. |
5 | Heating and cooling setpoints. To change the active setpoint, click the arrow buttons. |
6 | Humidity |
7 | Temperature |
Note: Devices that support energy saving features display the energy saving status, and
if setpoints are not in their optimal settings, you can click a button to reset
them.