Introduction to Verasys - Verasys - LIT-12013613 - LC-SBH200-0 - Building automation software - Verasys System - 4.0

Verasys Tenant User Guide

Brand
Verasys
Product name
Verasys System
Document type
User Guide
Document number
LIT-12013613
Version
4.0
Revision date
2020-09-30
Product status
Active
Language
English

The Verasys system provides bundled equipment and controls solutions that are well-proven. Verasys is part of the Johnson Controls® SMART Systems. The Verasys system features both simple, configurable controllers and HVACR equipment from the factory or installed in the field. You can use Verasys to configure many HVACR controls applications for one building or an entire enterprise comprised of multiple buildings, without using special programming tools or control engineering.



Verasys has a key role in the Internet of Things (IoT) ecosystem in the light commercial market. The technology is based on the SMART equipment technology and uses the core assets of Johnson Controls Metasys product lines. You can use Verasys to create installation use cases that provide standard feature sets for the light commercial space.