For information about the spaces on the Refrigeration tab, see the following figure and table.
Figure 1. Facility refrigeration tab
Callout | Description |
---|---|
1 | The refrigeration status. It can be on or off. |
2 | The defrost status. It can be on or off. |
3 | The defrost setting, and a link to the home page of the device and
buttons to access the device alarms and trends. Note: You cannot change
the defrost setting.
|
4 | The refrigeration setpoint. To change the setpoint, click the arrow buttons. |
5 | Temperature |