To access detailed information about a device, choose one of the following options:
-
Click the Devices menu, and on the Devices page, click the box of a device.
-
Select the device from the Choose a device drop-down menu at the top of the menu bar.
The device menu contains the following items:
-
Home Page
The device home page contains a device graphic, a circle of comfort, alarms, and key parameters. The content of the home page depends on the options that the device supports.
Note: You cannot modify the device graphic. -
Alarms
Alarm information is available if the device supports alarms. On the Alarms page, you can view two alarm lists:- To view the active alarms, click Active Alarms.
- To view the last 50 alarms on the device, both the active and the inactive ones, click All Alarms.
To sort the alarm list, click the column headers.
-
Trend
Trend information is available if the device supports trend objects. Trend objects contain trend points. The Verasys system reads a configurable amount of data from the trend points at configurable intervals.
On the Trend page, you can see a list of all available trend objects in the navigation bar.
To view a graphical display of the data from a trend point, click the trend object, and then click the trend point.
To download the trend data, click Download as CSV.
-
Schedule
Device schedules are available if the device supports the scheduling functionality. For information about how to set schedules, see Setting schedules.