The Facility screen appears when you log in to the SBH. In the Facility screen, you can see the status for all the spaces on the site that Verasys devices supervise, and change setpoints and other parameters. For more information, see the following figure and table.
Figure 1. SBH Facility screen
Callout | Description |
---|---|
1 | Facility name |
2 | Tabs for the following categories of spaces:
|
3 | Spaces in collapsed view. For more information about a
space, expand the row of the space. Note: The information that you can see for a space depends
on the type of the device that controls the space and the features
that the device supports.
|