Sensor bus port - Verasys - Bulb controller - Verasys Equipment Controller

Verasys Equipment Controller (VEC) Installation Guide

Product
Controls > Application Controls > Verasys Equipment Controller
Document type
Installation Guide
Document revision
C
Revision date
24/02/2020
docpartnumberlabel
Part No.
Part number
24-10143-1272

The sensor bus port on the top left side of the controller is an RJ-12, 6-position modular jack that provides a connection for specified network sensors with RJ-12 plugs. The terminal block method of connecting the devices to the sensor bus is the recommended method. The application does not prevent you from using this connection, if the correct device is used.

Figure 1. Sensor bus port
Table 1. Pin number assignments for the sensor bus port
6 Power (15 VDC)
5 Bus and power common
4 Power (15 VDC)
3 Bus and power common
2 Sensor bus -
1 Sensor bus +