Stacked zone bus and sensor bus terminal block - Verasys - Bulb controller - Verasys Equipment Controller

Verasys Equipment Controller (VEC) Installation Guide

Product
Controls > Application Controls > Verasys Equipment Controller
Document revision
C
Revision date
2020-02-24
Product status
Discontinued
docpartnumberlabel
Part No.
Part number
24-10143-1272

A dual-stacked connector serves as the zone bus and sensor bus port on the VECs. The upper row on the connector is the zone bus port. The lower connector row is the sensor bus port.

Figure 1. Stacked zone bus and sensor bus terminal block

The zone bus connects to the zone bus of the Verasys Zone Coordinator (VZC). The sensor bus connects to additional sensors.