The sensor bus terminal block is a brown, removable, 4-terminal plug that fits into a board-mounted jack.
Wire the removable sensor bus terminal block plugs on the lower port of the dual stacked connector to the controller, and other sensor bus devices in a daisy-chain configuration using a 4-wire twisted, shielded cable as shown in the following figure. See Table 1 for more information.
Figure 1. Sensor bus terminal block wiring
1 | Terminating device on the sensor bus |
2 | Sensor bus terminal block plug on the terminating device |
3 | Daisy-chained device on a sensor bus segment |
4 | Sensor bus terminal block plug on the daisy-chained device |
5 | Cable shield connection |
6 | Connects to the next device on the sensor bus. |
Note: The PWR terminal supplies 15 VDC. The PWR terminal can be used to connect (daisy
chain) the 15 VDC power leads on the sensor bus.