Maximum Cable Length versus Load Current - Verasys - Bulb controller - Verasys Equipment Controller

Verasys Equipment Controller (VEC) Installation Guide

Product
Controls > Application Controls > Verasys Equipment Controller
Document revision
C
Revision date
2020-02-24
Product status
Discontinued
docpartnumberlabel
Part No.
Part number
24-10143-1272

Use the following figure to estimate the maximum cable length relative to the wire size and the load current (in mA) when wiring inputs and outputs.

Note: The following figure applies to low-voltage (<30V) inputs and outputs only. The required wire size and length for high-voltage (>30V) Relay Outputs is determined by the load connected to the relay and local electrical codes.
Figure 1. Maximum Wire Length by Current and Wire Size