Wiring - PENN Controls - LIT-125118 - A25CN - A25AN - A25CP - Electromechanical Temperature Control - A25 Warm Air Limit Control

A25 Series Warm Air Control with Manual Reset Product/Technical Bulletin

Product
Controls > Air Handling and Air Controls > A25 Warm Air Limit Control
Document type
Product Bulletin
Technical Bulletin
Document number
LIT-125118
Document revision
C
Revision date
2021-09-29
Part number
24-7664-656
WARNING
  • Shock hazard
  • To avoid electrical shock or damage to equipment, disconnect all power before making wiring connections.

If available, follow the instructions for the unit onto which the A25 will be installed. Make all wiring connections only with copper conductors and in accordance with the National Electrical Code and local regulations. Refer to the label inside the A25’s cover for the maximum electrical rating.