Procedure
- After completing the installation and wiring procedures, turn on the power to the circuit.
-
Turn the setpoint knob counterclockwise until the A25 shuts down the system.
The A25 should lockout and the alarm or signal (if applicable) should
activate.
Note: The setpoint at shutdown should equal the approximate duct air temperature.
- Turn the setpoint knob clockwise to the desired setpoint. Nothing should happen.
- Press the reset lever. The system should restart and the alarm or signal (if applicable) should shut off.