Checkout procedure - PENN Controls - LIT-125118 - A25AN - A25CN - A25CP - Electromechanical Temperature Control - A25 Warm Air Limit Control

A25 Series Warm Air Control with Manual Reset Product/Technical Bulletin

Product
Controls > Air Handling and Air Controls > A25 Warm Air Limit Control
Document type
Product Bulletin
Technical Bulletin
Document number
LIT-125118
Document revision
C
Revision date
2021-09-29
Part number
24-7664-656

After installing the A25, perform the following procedures. Observe at least three complete operating cycles to verify that all components are functioning properly. If the unit fails to checkout, refer to the troubleshooting chart (Table 1). Do not attempt to make adjustments.