The following tables provide information about the Verasys application coverage.
Feature | Simplicity Smart Equipment | 3rd party controller (VEC100) |
---|---|---|
Up to four stages of cooling |
Yes |
Yes |
Modulated cooling |
No |
Yes |
Up to two stages of heating |
Yes |
Yes |
Up to three stages of heating |
Yes |
No |
Modulated heating |
Yes |
Yes |
Heat pump |
Yes |
Yes |
Economizer |
Yes |
Yes |
Title 24 economizer
Note: 24 sequence and alarm notification is
implemented from within the application. State of California
certification is pending.
|
Yes |
No |
Demand ventilation control |
Yes |
Yes |
Dehumidification |
Yes |
No |
Humidification |
No |
No |
Variable frequency drive for COBP |
Yes |
Yes |
Feature | Simplicity Smart Equipment | TEC36xx | LC-VAC1000-0 | LC-VAC3000-0 |
---|---|---|---|---|
Up to two stages of cooling |
Yes |
Yes |
Yes |
Yes |
Up to four stages of cooling |
Yes |
No |
Yes |
Yes |
Modulated cooling |
No |
No |
Yes |
Yes |
Up to two stages of heating |
Yes |
Yes |
Yes |
Yes |
Up to three stages of heating |
Yes |
No |
Yes |
Yes |
Up to four stages of heating |
No | No | Yes | Yes |
Heat pump |
Yes |
Yes |
Yes |
Yes |
Economizer |
Yes |
Yes |
Yes |
Yes |
Title 24 economizer
Note: Supports the five standard economizer
faults specified by Title 24 Part 6, Section 120.2(i) of the
California Code of Regulations. Thermostat control genrates
a service alarm in BACnet and N2 communication modes for the
following conditions:
|
Yes |
Yes |
Yes |
Yes |
Demand ventilation control |
Yes |
Yes |
Yes |
Yes |
Dehumidification |
Yes |
Yes |
Yes |
Yes |
Humidification |
No |
No |
Yes |
Yes |
Fixed variable fan |
Yes |
No |
Yes |
Yes |
Feature | LC-ZEC510-1 |
---|---|
Up to three stages of box heat |
Yes |
Incremental valve for box heat |
Yes |
Proportional signal for box heat (SCR or valve) |
Yes |
Supports no fan |
Yes |
Supports series fan |
Yes |
Supports parallel fan |
Yes |
Discharge temp monitoring |
Yes |
Occupancy sensing input |
Yes |
Up to eight net sensors (averaging) |
Yes |
Up to five CO2 sensors (high select) |
Yes |
Staged supplemental heat |
Yes |
Incremental supplemental heat |
Yes |
Feature | LC-ZEC310-0 |
---|---|
Modulated box heat |
Yes |
On/Off box heat |
Yes |
Modulated supplemental heat |
Yes |
PWM supplement heat (10 sec duty cycle) |
Yes |
On/Off supplemental heat |
Yes |
Occupancy sensing input |
Yes |
Up to eight net sensors (averaging) |
Yes |
Up to five CO2 sensors (high select) |
Yes |
Extra output for second damper actuator |
Yes, see note below |