Locations or applications that prohibit cellular telephones or Wi-Fi systems are unsuitable for the wireless Verasys products. For example, the following locations:
- Operating rooms or radiation therapy rooms
- Validated environments
- UL 864 applications
- Department of Defense applications requiring Defense Information Assurance Certification and Accreditation Process, such as military bases and military hospitals
Do not use the wireless products in applications that cannot tolerate intermittent interference, or in the following situations:
- Critical control features that impact life-safety or result in large monetary loss, including secondary backup
- Life-safety applications
- Data centers, production lines, or critical areas that shut down
- Loss of critical control that results from loss of data from humidity or temperature sensor communications
- Operating exhaust fans or AHUs that impair a purge or pressurization mode
- When missing data invalidates reporting required by the customer or regulatory authority
- Monitored security points