You can use the temperature setback feature to establish setback temperature On and Off values.
When the user-supplied switch closes the binary input control
circuit, the LCD displays BIN
in the
upper-right corner and the controller controls the output relay
load to these effective setback values.