The following figures show the dimensions of the A421 control with Type 1/IP20 enclosure.
Figure 1. A421ABx and A421GBx controls, dimensions, in. (mm)
Figure 2. A421ABJ control with one power cord, dimensions, in. (mm)
Figure 3. A421ABG control with two power cords, dimensions, in. (mm)