Adjustable sensor offset - PENN Controls - LIT-12011972 - A421ABC - A421ABG - A421ABJ - A421AEC - A421AEJ - A421GBF - A421GEF - Electronic Temperature Control - A421 Standard Model

A421 Series Standard Electronic Temperature Controls with and without Power Cords Product Bulletin

Brand
PENN Controls
Product name
A421 Standard Model
Document type
Product Bulletin
Document number
LIT-12011972
Revision date
2023-01-09
Language
English

Use the sensor temperature offset feature to offset the temperature displayed on the LCD from the temperature sensed at the A99 sensor. This feature is useful when the displayed temperature is different from the temperature measured at the sensor.