The sensor failure mode defines how the A421 control operates the
equipment in the event of a sensor or sensor-wiring failure. The
A421 control can be set to run the equipment continuously or to
shut it down if the sensor or sensor wire fails. When a failure
is detected, SF
flashes alternately with
OP
on the LCD if the sensor circuit
is open, or SF
and SH
if the
sensor circuit is shorted.