View the status, parameters, temperature, units, operating mode icons, and binary input on the LCD. The flame icon indicates heating mode. The snowflake icon indicates cooling mode.
You can set up the parameters and adjust the control with the three-button touchpad on the front panel. Use the Menu button to save values and advance to the next parameter.
The green LED indicator illuminates when the output relay is closed.