You can use the temperature setback feature to establish setback temperature On
and Off values. When the user-supplied switch that is connected
between the BIN and COM terminals closes, the LCD displays
BIN
in the
upper-right corner and the controller controls the output relay
load to these effective setback values.