Use the A421 Control with Off-Cycle Defrost to set up regular, passive defrost periods of 1 minute to 99 minutes. The defrost interval can range from 2 hours to 24 hours, or you can set it to 0 for no defrost interval. You can also start or stop a defrost cycle in two ways: you can use the three-button touchpad on the advanced menu or connect a momentary switch to the binary input (BIN). See Figure 1 through Figure 3.