- Off-cycle defrost
- Shut off the refrigeration system for a defined defrost time interval and frequency. You can also start or stop a manual-only defrost off-cycle.
- Control front panel LCD
- Displays the temperature, parameters, and status. You can adjust the backlight brightness for ambient light conditions. Custom icons display the system and control status.
- Basic and advanced programming menu
- Provides two levels of parameter adjustment and control. You can set up advanced features in one menu and easily adjust basic parameters in the other menu.
- On and Off temperature adjustment
- Select the temperature values at which the relay turns on and off, which automatically defines the mode of operation.
- Switch-activated temperature setback
- Shift the On or Off temperature by an adjustable setback. When a user-supplied switch closes the binary input control circuit, temperature setback is enabled.
- Adjustable anti-short cycle delay
- Select the minimum time the output relay remains off before the next on-cycle. By selecting this minimal time, you can avoid short cycling, hard starts, and nuisance overload outages on compressors and other inductive applications.
- Adjustable sensor offset
- Adjust the displayed temperature to the actual sensed temperature.
- Optional restricted adjustment mode
- Restrict On or Off adjustment to your defined temperature range.
- Sensor failure mode
- Run the control continuously in the event of a sensor or sensor wire failure or shut it down.
- Backlight brightness level
- Adjust the LCD backlight intensity. You can apply the backlight brightness level during normal operation. When you set up or adjust the parameters, the LCD automatically goes to the brightest level.