If you plan to install the Metasys Advanced Reporting System, first complete the following tasks:
- Install SQL Server Reporting Services. For more information, see Installing SQL Server Reporting Services for SQL Server 2019 and SQL Server 2017.
- Address specific system requirements, see Specific system requirements for the Metasys Advanced Reporting System.
- Configure SQL Server Reporting Services, see Configuring SQL Server Reporting Services.
- Verify the SQL Server Reporting Services configuration, see Verifying SQL Server Report Server configuration.
- Install Microsoft Report Viewer 2012, for more information, see Installing Microsoft Report Viewer 2012 redistributable package.