Procedure
- Using a supported web browser, browse to the Microsoft Download Center website: www.microsoft.com/downloads
-
Download the language-specific Microsoft Report Viewer Language Pack from the Microsoft Download Center website for your particular version of SQL Server software by following these steps:
- For SQL Server 2016, SQL Server 2014, or SQL Server 2012 software, use the Search field to look for Microsoft Report Viewer 2012 Language Pack.
- After you click Search, select the appropriate Microsoft Report Viewer Language Pack for your version of SQL Server software.
- On the Microsoft Report Viewer Language Pack page, select a language from the Select Language drop-down list box.
- Click Download. The page now appears in the language you selected in Step c.
- Click Download and save the file to a location on your computer. The language pack that downloads matches the language you selected in Step c.
- Run the downloaded file to install the language pack.
- Repeat Step c through Step f for any service packs (if available) and any other languages you want to support.
- Restart the computer.
-
If the computer has the ADX/ODS software installed, log in to the Metasys Advanced Reporting System with the credentials of a non-English user.
If the computer does not have the ADX/ODS software installed, come back to this section after the ADX/ODS is installed to perform the verification step (Step 4).
-
Verify the language appears correctly in the reporting system main
Toolbar and Report Toolbar.
Also verify the Report is being generated message that
appears in the Report screen is in the desired language.
Note: For content to appear in a language other than English, you also must have the correct language files on the ADX/ODS and the language defined in the non-English user’s Security Administrator System profile. These requirements are the same for an ADX/ODS without the reporting system.