The following information is new or revised:
- Added support for SQL Server® 2019 (64-bit).
- Removed support for SQL Server® 2012.
- Removed support for SQL Server Express® 2012.
- Metasys Advanced Reporting System and Energy Essentials does not support SQL Server 2019.
- The latest available version of the Open Data Server (ODS) is Release 10.1. The ODS is not available for upgrade to Metasys Release 11.0.