Specific system requirements for the Metasys Advanced Reporting System - Metasys - LIT-12012240 - Server - SQL Server - 11.0

SQL Server Installation and Upgrade Guide

Brand
Metasys
Product name
SQL Server
Document type
Installation Guide
Document number
LIT-12012240
Version
11.0
Revision date
2021-02-05
Product status
Active
Language
English

About this task

If your system is a split ADX using a web or application server or uses Reporting Services that were added to a previous installation of SQL Server software, complete these steps:

Procedure

  1. Create a new SQL Server software user for the Metasys Advanced Reporting System. For a split ADX, create the user on the web or application server. See Creating a new SQL Server user.
  2. Configure the SQL Server Reporting Services software. See Configuring SQL Server Reporting Services.
    This section uses Microsoft software default values in many cases. These settings are sufficient for LAN network security. For advanced users who want enhanced network security not presented in this section, refer to http://www.microsoft.com