The ZFR1825 Coordinator has five LEDs that indicate power, fault status, FC Bus activity, wireless activity, and signal strength. See Figure 1. These status LEDs are described in Table 1.
Name | Color | Normal | Descriptions |
---|---|---|---|
Power |
Green |
On |
Off Steady = No power. On Steady = Normal operation (power available from 24 VAC connector or Field ControllerSensor Actuator [FC/SA] Bus IN jack). |
Fault |
Red |
Off |
Off Steady = Normal. On Steady = Internal Errors detected. |
FC Bus |
Green |
Blink |
Blink - 2 Hz = Normal operation (ZFR1825 Coordinator is receiving BACnet® frames over the wire). Off Steady = Attempting to Auto Baud, or not connected to active MS/TP network. On Steady = Auto Baud complete and not receiving BACnet frames. |
Wireless |
Green |
Blink |
Blink - 2 Hz = Normal operation (ZFR1825 Coordinator is receiving BACnet frames over the wire). Off Steady = Not receiving BACnet frames. On Steady = Stopped receiving BACnet frames. |
Signal Strength |
Green |
Signal Strength 1 Indication: 3 Flashes - Excellent 2 Flashes - Good 1 Flash - Weak OFF for 3 seconds - None |
OFF Steady = Not able to start a network. ON Steady with Signal Strength displayed once every 10 seconds = Normal operation (ZFR1825 Coordinator is a member of a wireless network). 5 Rapid Flashes = Network has been started, but no other ZRF Pro devices are seen. |