Network Optimize/Reform Button - Verasys - Wireless Device - ZFR1800 Series Wireless Field Bus System

ZFR1825 Wireless Field Bus Coordinator Installation Guide

Brand
Verasys
Product name
ZFR1800 Series Wireless Field Bus System
Document type
Installation Guide
Part number
24-10325-00142
Document revision
Revision date
2019-12-02
Language
English

The Network Optimize/Reform Button allows the ZFR1825 Coordinator to use any of three functions:

  • Signal Strength
  • Network Optimize
  • Network Reform

Use the Signal Strength mode to aid in signal strength testing. Signal Strength mode causes the LEDs on the ZFR Pro routers to turn on and display signal strength for two hours.

Use the Network Optimize mode to clear the mesh device routing tables of the ZFR Pro Routers and attempt to find shorter and/or stronger signal paths to the ZFR1825 Coordinator.

Note: The Network Optimize process can take up to 15 minutes to complete.

Use the Network Reform if new ZFR Pro or WRZ devices are failing to join the ZFR Pro Mesh network. Refer to the Verasys Wireless Pro System Technical Bulletin (LIT-12012940) for more information about the Network Reform function.

Table 1. Network Optimize/Reform Button
Holding the Network Optimize/Reform Button for ___ Puts the ZFR1825 Coordinator into the _____ Mode

0–5 Seconds

Signal Strength

5–10 1

Network Optimize

More than 10 2

Network Reform

1 Once the Signal Strength LED begins blinking rapidly, release the button (between 5 to 10 seconds).
2 Once the Signal Strength LED stops blinking rapidly and stays ON, release the button (approximately 10 seconds).