Assembling the Antenna - Verasys - Wireless Device - ZFR1800 Series Wireless Field Bus System

ZFR1825 Wireless Field Bus Coordinator Installation Guide

Brand
Verasys
Product name
ZFR1800 Series Wireless Field Bus System
Document type
Installation Guide
Part number
24-10325-00142
Document revision
Revision date
2019-12-02
Language
English

About this task

Important: Use the antenna provided. Do not alter the antenna in any way or use another antenna. Do not modify the antenna cable in any way.
Important: Minimum bend radius for the antenna cable is 25 mm (1 in.). Any bend with a smaller radius may damage the cable.

If mounting the ZFR1825 Coordinator in a control panel, choose a location on the top side of the control panel for placement of the antenna. Ensure that the selected location has line-of-sight to two or more ZFR Pro Routers.

Use Figure 1 and the following steps to assemble the remote-mount antenna.

Procedure

  1. Remove the knock-out tab on the enclosure/panel box or drill a 7/8 in. diameter hole in the desired location on the top of the enclosure.
  2. Insert the round bushing into the hole in the enclosure.
  3. Insert the hexagonal bushing into the antenna mounting bracket.
  4. Thread the antenna cable through the hexagonal bushing.
  5. Insert the base of the antenna into the hexagonal bushing and press until it snaps securely in place.
  6. Thread the antenna cable through the round bushing at the top of the panel.