About this task
The ZFR1825 Coordinator can be surface mounted using the four No. 6 Trade Size self-tapping, pan-head screws supplied.
Procedure
To mount the ZFR1825 Coordinator base with screws, complete the following steps:
The ZFR1825 Coordinator can be surface mounted using the four No. 6 Trade Size self-tapping, pan-head screws supplied.
To mount the ZFR1825 Coordinator base with screws, complete the following steps: