Procedure
CAUTION
- Risk
- Turn off the liquid supply and relieve the pressure before
installing or removing the bulb or bulb well.
For liquid immersion applications where you can remove the temperature bulb
without draining the tank you can use a bulb well.
-
Install the bulb well in the tank opening.
-
Remove the bushing from the bulb well and slide the bushing over the
capillary.
-
Insert the bulb into the bulb well and replace the bushing.
-
Push the bulb into position in the bottom of the well.
-
Tighten the set screw in the adapter end to hold the bulb in position.
Figure 1. WEL14A-600R bulb well