Information | Description |
---|---|
Purpose of the control | Temperature control |
Method of mounting the control |
Flat surface mounted. The bracket is on the back of the case. |
Method of grounding the control | Wiring binding screw terminal |
Type 1 or Type 2 action | Type 1.B micro-disconnection |
External pollution situation | Pollution degree 3 |
Rated impulse voltage | 4,000 VAC |
Compliance |
File SA516 UL Guide No. SDFY cUL Guide No. SDFY7 |