Mounting - PENN Controls - LIT-121071 - A19ZBC-10C - A19ZBC-12C - A19ZBC-6C - Electromechanical Temperature Control - A19 Control for Hot Water Immersion
A19ZBC Temperature Control Installation Guide
- Brand
- PENN Controls
- Product name
- A19 Control for Hot Water Immersion
- Document type
- Installation Guide
- Document number
- LIT-121071
- Part number
- 996-460
- Document revision
- C
- Revision date
- 2023-10-04
- Language
- English
Procedure
-
Use the mounting bracket as a template and
mark the location for the two mounting
screws.
-
Drill or punch two holes and start the
mounting screws.
-
Place the slot in the bottom of the bracket
under the head of the lower mounting screw.
-
Position the control so that the top screw is
in the top slot.
-
Tighten both screws. It is not necessary to
level the control except for appearance.