North American emissions compliance - Verasys - LC-VAC1000-0 - VAC1000

Constant Volume Controller Quick Start Guide LC-VAC1000-0

Brand
Verasys
Product name
VAC1000
Document type
Quick Start Guide
Part number
24-10143-01841
Document revision
A
Revision date
2020-02-25
Language
English

United States

This equipment has been tested and found to comply with the limits for a Class A digital device pursuant to Part 15 of the FCC Rules. These limits are designed to provide reasonable protection against harmful interference when this equipment is operated in a commercial environment. This equipment generates, uses, and can radiate radio frequency energy and, if not installed and used in accordance with the instruction manual, may cause harmful interference to radio communications. Operation of this equipment in a residential area may cause harmful interference, in which case the users will be required to correct the interference at their own expense.

Canada

This Class (A) digital apparatus meets all the requirements of the Canadian Interference-Causing Equipment Regulations.

Cet appareil numérique de la Classe (A) respecte toutes les exigences du Règlement sur le matériel brouilleur du Canada.